0 items

Tricks of the Trade

Floor cleaning and maintenance tips

Melissa Paniagua, a Ferguson Website Content Coordinator

by Melissa Paniagua

 

As the old saying goes, an ounce of prevention is worth a pound of cure. This definitely applies to the flooring in your facility, where dust and grit can act as an abrasive on hard and soft surfaces alike. Regular cleaning and maintenance can extend the life and look of your floors, so you can avoid spending your repair budget on unnecessary flooring replacement costs. Use these tips to help you save resources by preserving your VCT, ceramic, terrazzo, concrete, carpet floors and matting.

VCT (Vinyl Composition Tile)

As needed:

  • Remove finish (if any).
  • Dust mop and clean with an 4:1 emulsifier solution.
  • Apply to floor and allow to dwell for 15 minutes.
  • Agitate with floor machine and black pad, remove with wet vac.
  • Check floor thoroughly for any missed spots.

Helpful tip: For new floor, check with the installer for appropriate cure times before applying excess cleaning solutions or floor strippers.

Concrete

Daily:

  • Keep free of debris and dust using a dust mop.
  • Cleanse concrete with a low suds cleaner and an automatic scrubber, the most productive and economical choice for cleaning concrete floors.

Helpful tip: Automatic scrubbers are sized to the total area of the facility and the width of any areas needed to be cleaned. Larger units may be used for open areas and rider scrubbers increase productivity.

Get the janitorial supplies you need now >>
 

Terrazzo

Daily:

  • Dust mop or broom sweep. Use a good mating program to keep most dirt localized at the door and prevent it from grinding down the coating. Dust/mop up dirt that does get inside.

Weekly:

  • Wet mop with all-purpose cleaner.

Pro tip: The type of mop you use can make a significant difference in the overall cleanliness of your facility. See how to pick the right mop >>

Quarterly:

  • Reseal floors with a water-based sealer.

Annually or Biannually:
Undergo a gloss restoration. Floor surface must be clean, dry and have all previous finish materials removed.

  • Dust mop floor with a dust mop system to remove all debris.
  • Strip all finish from the floor with a rinse-free stripper.
  • Prepare the clean floor surface with the recommended floor pad.
  • Apply a stone floor coating per label directions.

Ceramic Tile & Grout

Daily:

  • Clean with a traditional wet mop system, deck brush or automatic scrubber that utilizes cylindrical brushes. Avoid acidic cleaners.

Pro tip: The size and material of your wet mop should be taken into consideration when developing your cleaning system. Learn more >>

Biweekly:

Annually:

  • Reseal grout and apply according to label directions to a clean floor. Applying a grout impregnator will repel moisture and protect grout from soil, grease and oil.

Helpful tip: Seal tile upon installation before any other maintenance. This should be the only time you have to do this if the floor is maintained properly.

Carpet

Daily to Weekly:

  • Depending on traffic, vacuum with fresh filter bag for maximum airflow and effectiveness.
  • As Needed/Quarterly:
  • Remove residue (if any) with an extraction cleaner. Increase dilution ratios to compensate for the soil loading.
  • Encapsulation
    • The encapsulating chemical is brushed in, distributing it throughout the carpet pile, and allowed to dry. As it dries it crystallizes around the sticky, oily soils adhered to the carpet fibers causing them to release from the fiber.
    • In 20 minutes when they are dry (or at the next scheduled vacuuming) they can be vacuumed out.
  • Drying
    • After encapsulation utilize several carpet fans to dry the area before re-opening to foot traffic.

Helpful tip: High soil load areas need to be vacuumed with upright vacuums with brush bar agitation.

Matting

Daily:

  • Vacuum to remove any dirt and debris trapped by matting.

Seasonally (winter/early spring):

  • If you can see that telltale whitish haze after vacuuming, this means that matting is full of ice melt residues that need to be removed.
  • Manual Process:
    • Dilute an all-purpose cleaner at 1-2 ounces per gallon.
    • Work it into the surface with the brush.
  • Extractor Process:
    • Use an extractor with an encapsulating chemical to flood the matting. Wait about 10-15 minutes of dwell time, and then extract the solution.
    • Check the water in the recovery tank. If it’s still dark and dirty, repeat until the extracted water is clear.

Helpful tip: When extracting, allow the cleaning solution to flood the matting by using your extractor without the vacuum engaged. This gives ample time to dissolve the salt residues and to break up and suspend oily soils.

Bonus tips:

  • As always, pay special attention to high-traffic areas like entrances, lobbies and busy hallways.
  • Consider using floor mats for high traffic areas on all flooring types. They will be your first line of defense against soils and substances tracked inside of your building.
  • Be on the lookout for buildup from soaps and cleaners that can make the floor slippery. Rinse the problem areas with water as needed.

  • Shop floor cleaning now >>

Mop selection guide

Incorporating the right selection of mops in your facility’s cleaning system is a key part of developing an effective floor care plan. Use our mop buying guide to pick the right mop and keep your facility clean.

  • Mop size makes a difference. Mops come in sizes ranging from small to extra large. These sizes are based on the amount of water the mop can hold. While some might assume that a larger mop provides greater cleaning power, this is not always true. The size of the mop should fit the size of the worker using it. Stock up on mop heads in a variety of sizes to make sure there’s a mop to fit everyone on your cleaning and maintenance crew.
  • Consider the material. Different mop materials offer different advantages. For facilities without laundry capabilities, a cotton mop is ideal for single use. Mops made from rayon or a rayon-cotton blend can be washed and reused. If your facility is equipped with laundry capabilities, this can save on operating expenses in the long run. Microfiber mops are a sound investment because they are washable and require less water and cleaning solution to wash a surface, making them lightweight and efficient.
  • Keep construction in mind. How a mop is made affects its ability to clean effectively. Look for a mop that has looped ends to ensure thorough coverage. A mop with a tailband, which is a stitch at the bottom of the mop above the loops, will give the user more control over the mop. Mops that don’t have cute ends are inexpensive and lightweight, but typically not reusable.

    Buy mops online >>

    Consider Ferguson Facilities Supply your one-stop shop for all of your janitorial and MRO product needs. We have the product selection and the knowledge to help you implement an effective cleaning system in your facility.

Melissa Paniagua, a Ferguson Website Content Coordinator

Melissa Paniagua

Melissa's mission is to empower Ferguson customers in finding the resources they need to expand their knowledge through her writing. She has intensive experience in the creation of relevant industry content and aims to offer you meaningful insight and inspiration to help you better complete your next project.