How To Use Pro Pick-Up

  • Overview
  • Locating Pro Pick-Up
  • Selecting Pro Pick-Up
  • Checkout
  • Pro Pick-Up Details

Overview

Order ahead and pick up in store to get the products you need faster and have your online order waiting for you with the convenience of Pro Pick-Up. If you have a commercial credit account with Ferguson, you can take advantage of Pro Pick-Up or Pro Pick-Up with one-hour service (where available) to help save time and money in addition to choosing standard order delivery. Ferguson puts you in control by giving you multiple delivery and pick-up options that best fit your needs.

shopping cart image

You can select Pro Pick-Up right in your shopping cart during the checkout process. Simply order ahead online, select Pro Pick-Up or Pro Pick-Up with one-hour service in your shopping cart during checkout and your order is ready when you arrive. Pro Pick-Up helps you get what you need so you can get the job done.

Locating Pro Pick-Up

There are two convenient options to place an order for Pro Pick-Up in store.

order summary image

1. Online at ferguson.com

When placing your order online, locate the Pro Pick-Up or Pro Pick-Up with one-hour service option for your order pick-up in the Order Summary box before selecting Checkout.

phone orders image

2. By phone

You can also place your order over the phone at your local Ferguson and simply let them know you want to pick up your order. To find the phone number for your store, access your Dashboard under Account and scroll down to My Store for the address and phone number of your local store.

Selecting Pro Pick-Up

Pro Pick-Up is located in the Order Summary of your Shopping Cart. There are two Pro Pick-Up selections to choose from before you begin the Checkout process.

pro pick-up image

1. Pro Pick-Up

Select “Pro Pick-Up” for those orders you wish to pick-up at a Ferguson location. There are specific hours during which your order will qualify for Pro Pick-Up, so please check with your sales associate for more details.

one hour service image

2. Pro Pick-Up with one-hour service

You can get your Pro Pick-Up order in as fast as one hour at select locations. Choose the Pro Pick-Up option with the “1 Hour” indicated next to it in order to have your order ready and waiting for you. Pro Pick-Up with one-hour service is available during select times. Please check with your local Ferguson to see if this service is offered in your area.

pro pick-up in shopping cart image

Selecting Pro Pick-Up in your Shopping Cart

Select “Pro Pick-Up” in the Order Summary box of the Shopping Cart to see the store location where you will pick up your order. Once Pro Pick-Up is selected, click “Checkout” to begin the checkout process.

pick up location image

If you want to place a Pro Pick-Up order at another location, you may change the “Selected Store” location at the top of the Shopping Cart or Checkout page.

order summary pick up image

Selecting one-hour service for your Pro Pick-Up order in your Shopping Cart

You may select the “1 Hour” Pro Pick-Up option in the Order Summary box of your Shopping Cart if this service is offered at your location. Once the “1 Hour” option is selected, you have the option to change your pick-up location using a dropdown menu of other locations in your area that offer one-hour service. Simply select a new location from the dropdown menu by clicking on the location name, or you can use the search box to search for a location that offers one-hour service. Once your new Pro Pick-Up location is selected, click “Checkout” to begin the checkout process.

Checkout

On the Checkout page, the “Pick Up From” box confirms the Pro Pick-Up selection you entered in the shopping cart as well as the pick-up address and the date by which you need to pick up your order.

Pro Pick-Up

You can click “View Store Info” to see the location address, phone and hours of operation. You can also change the “Needed By” date by clicking on the dropdown arrow next to the current date. If you want to change your Pro Pick-Up location, click “Change” in the upper right corner of the Pick Up From box.

pick up from image
view store information image
pick up from window image

The “Pick Up From” window will expand and allow you to edit the following:

  1. Store Location – Use the arrow to open the dropdown menu and select the store location for the Pro Pick-Up. You can also click “View Store Info” for an address and hours of operation for the location.
  2. Date Needed – Click the dropdown arrow next to the date needed to change your date.
  3. Add Contact Phone – Click “Add Contact Phone” to add a contact phone number.
  4. Add Instructions – Click “Add Instructions” to add instructions/notes to your Pro Pick-Up order.
  5. Pickup Complete – Check the “Pickup Complete” box if you want to pick up the order once all products are available.
view store information location image
view store information hours image

Once all changes are complete, select the “Use This Pickup” button to confirm your pick-up details or “Cancel” to cancel your changes.

one hour pro pick-up image

Pro Pick-Up with one-hour service

For Pro Pick-Up with one-hour service, you are required to add a Contact Name and Contact Phone in order to proceed with your Pro Pick-Up if one does not appear. You can also make changes to the “Pick Up From” information by clicking “Change”.

contact name and phone image

If a Contact Name and Contact Phone are not provided, enter them in the boxes to then confirm your pick-up information. Once the required information is entered, the “Use This Pickup” button will highlight and can be selected. Once you click “Use This Pickup”, your Pro Pick-Up location with one-hour service is confirmed and you can proceed with checkout.

Pro Pick-Up Details

Your Order Confirmation details will indicate a Pro Pick-Up order.

order confirmation image

Pro Pick-Up order confirmation

one hour confirmation image

Pro Pick-Up order confirmation for one-hour service

Here are a few Pro Pick-Up details to be aware of and may vary from one location to another.

  1. Pro Pick-Up orders can be placed on ferguson.com via the desktop, mobile or Ferguson app or with a phone call to your local branch.
  2. There are specific hours during which your order will qualify for Pro Pick-Up. The Pro Pick-Up ordering times vary by location, so please check those times at your desired location before placing your order.
  3. When you arrive at the location, where you pick up your order will also vary by location, so please ask your sales associate to determine your pick-up location. Curbside pick-up is also available at some locations.
  4. In addition to Pro Pick-Up, self-checkout is also an option in store at some Ferguson locations.